Support Center

Knowledge Base

145 Results

FAQ

What is the serial command to select a UVC video stream format (IR16 or colorized)?

Leggi la storia

FAQ

What is the standard warranty period for Tau2, Quark2, and Boson cameras?

Leggi la storia

FAQ

What is the Tau2 PCB Wearsaver and what does it do?

Leggi la storia

FAQ

What is the voltage on the legacy Photon serial port? Do I need to access the serial port for normal operation?

Leggi la storia

FAQ

What material is used for the sensor windows of FLIR's uncooled cameras? Does the window have an anti-reflection (AR) coating? Can these cameras image below 8µ?

Leggi la storia

FAQ

What methods are available to acquire digital data using legacy Photon?

Leggi la storia

FAQ

What power density will saturate the pixels on the legacy Photon camera?

Leggi la storia

FAQ

What voltages can I use on the Tau2 and Quark2 serial port?

Leggi la storia

FAQ

When changing to Manual AGC, what needs to be done to generate a useful image?

Leggi la storia

FAQ

Where can I get a cable that fits the Quark2 Cable Adapter board?

Leggi la storia

FAQ

Why do Boson, Tau2, and Quark2 cameras need Schedule B and HS numbers?

Leggi la storia

FAQ

Why does a thermal image suddenly turn bright or dark when a new object enters the scene?

Leggi la storia

FAQ

Why does FLIR offer OEM camera modules with and without shutters?

Leggi la storia

FAQ

Why doesn’t DDE appear to have an effect on AGC?

Leggi la storia

Scaricare

Why Thermal Imaging Makes ADAS and AV Platforms Safer

Per saperne di più

FAQ

Will a pixel kill tool be available for Boson users?

Leggi la storia

FAQ

Will the Movidius SDK be available to users?

Leggi la storia

FAQ

Will the Photon replicator board used for the Tau2 320 work with the Tau2 640?

Leggi la storia

FAQ

Will the VPC allow an image from Tau2, Quark2 to be displayed on a PC or is a video frame grab card needed?

Leggi la storia

FAQ

Would the VPC and the GUI allow a Tau2 or Quark2 camera to be directly connected to a PC or laptop?

Leggi la storia