Teledyne FLIR Selected as Thermal Camera Provider for the Red Cat Drone Black Widow U.S. Army SRR Program Award

/globalassets/industrial/oem/hadron-640r/redcat-blackwidow_articleheader.jpg

Integration of Prism Embedded Software and Hadron 640R+ Payload to Provide Cutting-Edge Thermal Sensing and Air-to-Ground AI Capabilities

 

GOLETA, Calif., Nov. 20, 2024— Teledyne FLIR, part of Teledyne Technologies Incorporated, today announced it has been selected by Red Cat Holdings, Inc., to provide thermal imaging and Artificial Intelligence (AI) embedded software for its Black Widow™ small unmanned aircraft system (sUAS). Red Cat was selected as the winner of the U.S. Army’s Short Range Reconnaissance (SRR) Program of Record after an evaluation process completed by the Army Project Management Office for Uncrewed Aircraft Systems, Army Maneuver Battle Lab, Army Test and Evaluation Command, and Army Operational Test Center.The U.S. Army’s current acquisition objective is for 5,880 systems, with each system consisting of two aircraft.

Red Cat incorporated Teledyne FLIR’s NDAA-compliant Hadron™ 640R+ longwave infrared and mega-pixel visible camera module and its Prism™ AI embedded perception software into Black Widow, a highly capable, rucksack-portable sUAS designed for operation in Electronic Warfare (EW) environments. Black Widow’s fully modular architecture enables swift adaptation to diverse mission requirements, including SSR and secondary payload operation.

“We are proud to be selected by Red Cat to support the Black Widow with unparalleled tactical capabilities for the U.S. Army’s SSR Program,” said Paul Clayton, Vice President, Teledyne FLIR. “This collaboration provides the Black Widow with superior yet compact dual thermal-visible imaging along with AI software libraries that enable classification, object detection, and object tracking to complete the mission day or night.”

​​“The Hadron 640R+, with its best-in-class thermal vision, will play a key role in helping the warfighter Dominate the Night™ with the Black Widow,” said George Matus, CTO of Red Cat. “We are thrilled to continue our longstanding relationship with the world leader in thermal imaging technology, enabling Red Cat to accelerate deployment to the U.S. DoD and its allies across the globe.”

The International Traffic in Arms Regulations (ITAR)-free Hadron 640R+ provides a 640x512-resolution thermal camera with industry-leading thermal sensitivity and a 64-MP resolution visible camera in a size, weight, and power (SWaP) optimized package. Paired with Prism AI embedded software, the combination can enable high-precision object detection within application-specific classes, multiple object tracking, motion target indication, and more.

Military+Aerospace Electronics magazine recently recognized Teledyne FLIR’s Prism digital ecosystem as a Platinum Honoree, its highest award for innovation in defense and aerospace.

To learn more about Teledyne FLIR, visit oem.flir.com.  

 

About Teledyne FLIR

Teledyne FLIR, a Teledyne Technologies company, is a world leader in intelligent sensing solutions for defense and industrial applications, with approximately 4,000 employees worldwide. Founded in 1978, the company creates advanced technologies to help professionals make better, faster decisions that save lives and livelihoods. For more information, please visit www.teledyneflir.com or follow @flir.

 

About Red Cat, Inc.  

Red Cat (Nasdaq: RCAT) is a drone technology company integrating robotic hardware and software for military, government, and commercial operations. Through two wholly owned subsidiaries, Teal Drones and Flightwave Aerospace, Red Cat has developed a bleeding-edge Family of ISR and Precision Strike Systems including Black Widow™, a small unmanned system offering the highest-resolution thermal imaging in its class, TRICHON™ Tricopter for extended endurance and range, and FANG™, the industry’s first line of NDAA compliant FPV drones optimized for military operations with precision strike capabilities. Learn more at www.redcat.red.

관련 기사