Teledyne FLIR Expands Next-Generation Hadron 640 Series of Dual Thermal-Visible Cameras for Unmanned Systems Integrators

/globalassets/industrial/oem/hadron-640r/hadron-640-series-article-header.jpg

Latest Hadron 640 Models Bring enhanced Thermal Sensitivity and SWaP-Optimized Design for Out-of-the-Box Integration

 

GOLETA, Calif. and PARIS, France — June 12, 2024 ― Teledyne FLIR, part of Teledyne Technologies Incorporated, today released its next generation of high-performance Hadron 640 dual radiometric thermal and visible camera modules. The ITAR-free Hadron 640+ and radiometric Hadron 640R+ provide industry-leading thermal sensitivity. All models are size, weight, and power (SWaP) optimized for integration into unmanned aircraft systems (UAS), unmanned ground vehicles (UGV), robotic platforms, and emerging AI applications utilizing Teledyne FLIR Prism™ software.

“The Hadron 640 series gives integrators the opportunity to deploy AI-ready, high-performance dual-camera modules into small unmanned systems where SWaP, performance, run time, and battery life are mission critical,” said Michael Walters, Vice President Product Management, Teledyne FLIR. “With Teledyne FLIR’s new Prism AI detection, tracking, and classification models and Prism ISP libraries offering super-resolution, turbulence mitigation, contrast enhancement, and more, Hadron 640 also enables effective AI-based applications.”

The new Hadron 640 modules include a 640 x 512 resolution Boson+ longwave infrared (LWIR) camera module with industry-leading thermal sensitivity of 20 millikelvin (mK) or better. It sees through total darkness, smoke, most fog, and glare allowing operational awareness day and night. The Hadron 640R+ provides temperature measurements for every pixel in the scene. The addition of a 64MP visible camera enables the Hadron 640 series to provide both thermal and visible imagery within a single camera module.

“Continued collaboration with Teledyne FLIR enables rapid payload and performance innovation for Teal drones, accelerates time to market, and equips warfighters with the best possible technology for operational success,” said George Matus, CTO of Red Cat. “The Hadron 640 series features enhanced thermal sensitivity and HD visible cameras to provide superior performance within a compact package for the support of our NATO allies and the U.S. Army’s Short Range Reconnaissance Tranche 2 program of record.”

To reduce development costs and time-to-market for integrators and original equipment manufacturer (OEM) product developers, the Hadron 640 series offers a complete system through a single supplier. This includes drivers for market-leading processors from NVIDIA, Qualcomm, and more, plus industry-leading integration support and service from a Teledyne FLIR support team of experts.

The Hadron 640 series products are all dual use and classified under US Department of Commerce jurisdiction. It is available for purchase globally from Teledyne FLIR and its authorized dealers. To learn more or to purchase, visit the Hadron product page.

For an exclusive in-person first look at the Hadron 640R+ running Prism AI, please visit hall 5A, stand #5A-127 at EuroSatory, June 17-21, 2024, in Paris, France.


About Teledyne FLIR 

Teledyne FLIR, a Teledyne Technologies company, is a world leader in intelligent sensing solutions for defense and industrial applications with approximately 4,000 employees worldwide. Founded in 1978, the company creates advanced technologies to help professionals make better, faster decisions that save lives and livelihoods. For more information, please visit www.teledyneflir.com or follow @flir.

相关文章