Knowledge Base
145 Results
Conseils techniques
What are the detection ranges for the various Tau2, Quark2 lens versions?
Lire le témoignageFAQ
What is needed to create my own application to control and or acquire digital data using Quark2 or Tau2?
Lire le témoignageFAQ
What is the damage threshold for Tau2 and Quark2 cameras? Can Tau2 and Quark2 cameras be used for LASER beam profiling?
Lire le témoignageFAQ
What is the difference between the PathFindIR II and Boson, Quark2, Tau2 cores?
Lire le témoignageFAQ
What is the I O module and how does it differ from going directly into a monitor or PC?
Lire le témoignageFAQ
What is the influence of the camera temperature on the pixel readings? Can this be corrected by a linear model?
Lire le témoignageFAQ
What is the line burst rate for the image data coming from the Tau2 640 camera? If the Camera Link accessory is used with the Tau2 640 camera, is the line burst rate the same?
Lire le témoignageFAQ
What is the MTBF for Tau2 and Quark2 cameras? Can FLIR provide any detailed analysis or test reports?
Lire le témoignageFAQ
What is the process for handling Boson, Tau2, and Quark2 warranty repairs, including typical turnaround times?
Lire le témoignageFAQ
What is the relationship between lens f-number and camera performance or NEdT?
Lire le témoignage