Support Center
Knowledge Base
145 Results
FAQ
What is the serial command to select a UVC video stream format (IR16 or colorized)?
Read the StoryFAQ
What is the voltage on the legacy Photon serial port? Do I need to access the serial port for normal operation?
Read the StoryFAQ
What material is used for the sensor windows of FLIR's uncooled cameras? Does the window have an anti-reflection (AR) coating? Can these cameras image below 8µ?
Read the StoryFAQ
Why does a thermal image suddenly turn bright or dark when a new object enters the scene?
Read the StoryFAQ
Will the VPC allow an image from Tau2, Quark2 to be displayed on a PC or is a video frame grab card needed?
Read the StoryFAQ
Would the VPC and the GUI allow a Tau2 or Quark2 camera to be directly connected to a PC or laptop?
Read the Story