Support Center

Knowledge Base

145 Results

FAQ

Does slow video have any effect on perceived resolution?

Read the Story

FAQ

Does Tau SWIR have radiometry (temperature measurement) features or options?

Read the Story

FAQ

Does Tau2 or Quark furnish an ability to wirelessly transmit or downlink video data from an unmanned vehicle or drone?

Read the Story

FAQ

Does the analog video format (NSTC, PAL) need to be specified when an order is placed for Quark2 or Tau2?

Read the Story

FAQ

Does the PathFindIR II come with the same accessories as Tau2 and Quark2 cameras?

Read the Story

FAQ

For Boson, Quark2, and Tau2 cameras used on vehicles for driver vision enhancement (DVE) or situational awareness, how would the operator inside view the scene?

Read the Story

FAQ

For protection, is a special window needed in front of my FLIR camera that won't interfere with the thermal imaging?

Read the Story

Technical Guidance

Heat Activated Power Strip with Lepton and WeMo

Read the Story

FAQ

How are FLIR's microbolometer arrays packaged? Are they under vacuum? Why?

Read the Story

FAQ

How are FLIR's thermal cameras identified for warranty tracking purposes? Is there a serial number, unique ID number, etc.?

Read the Story

FAQ

How does a neutral density filter affect the scene dynamic range of FLIR’s OEM cameras?

Read the Story

FAQ

How does FLIR calibrate thermal cameras? What is NUC?

Read the Story

FAQ

How does FLIR test its thermal camera cores and lenses for sealing to IP67? Is a vacuum test used?

Read the Story

FAQ

How does Tau2 adapt to the sense of the TTL output of a UART or RS-422 receiver?

Read the Story

FAQ

How far can I see with the PathFindIR II, Tau2, or Quark2?

Read the Story

FAQ

How is the Quark2 lens focused?

Read the Story

FAQ

How many bits per pixel is the digital output?

Read the Story

FAQ

I have lost or can’t find or don’t remember receiving the camera control software or User’s Guide. How can I get a copy?

Read the Story

FAQ

If the Photon Replicator Kit is used with Tau, is the Photon (Camera Control) GUI needed?

Read the Story

FAQ

Is faster video rate better than slow video for live streaming of thermal images?

Read the Story

FAQ

Is it possible to adjust the focus of Photon lenses manually? What is the range of focus? What is the close focus distance?

Read the Story

FAQ

Is it possible to image an object or scene that is hotter than the 550 C low gain scene range limit of Tau2 or Quark2?

Read the Story

FAQ

Is the (legacy) Photon tripod adapter necessary?

Read the Story

Application Note

Lepton Spot Meter Code

Read the Story

Others

Thermal Cameras for Safer AEB

Read the Story