Manufactured and sold by GroupGets, the ARM MCU JTAG Adapter can be used to flash and debug the PureThermal 1 system via JTAG by connecting the included ribbon cable to both board’s flat flex connectors (FFC). You will also need an ST-Link/V2 around connected over USB to flash/debug PT1. If you are planning on using this for another project make sure that it uses the same flat flex connector as this adapter.