Compare all our infrared camera core models in one place
By Camera Type
By Product Family
By Solution
By Product
You’ve added 1 of 10 models. Add another to start comparing.
To Compare:
145 results
FAQ
Can a Tau2 or Quark2 simply be connected to power and a video display?
System Requirements
Can any of FLIR's Camera Control software run on a Mac?
Can any of the default Lepton configurations be changed?
Can auto-exposure be turned on and off in Boson? Is auto-exposure used to normalize the image with respect to min and max pixel magnitude?
Can Boson, Tau2, Quark2 cameras be pointed at the sun?
Can FLIR provide the SDK documentation, or a list of functions controlled by the SDK, so we can make a decision on whether to order it?
Can FLIR supply a thermal sensor without an IR window? Or, with a custom window? If not, how difficult is it to remove the window?
Can I convert 8-bit AGC’d data to temperature in manual AGC mode?
Can lenses be interchanged on FLIR cameras? Will FLIR calibrate my lens with a Tau2 or Quark2?
Can researchers with foreign nationality use a Boson, Tau2, or Quark2 camera at our facility in the U.S.?
Can the FLIR start-up splash screen be disabled in Tau2 and Quark2 cameras? Can a different splash screen be used?
Can the lens focus be adjusted on Quark2, Tau2, and legacy Photon cameras?
Can the USB port on the Tau2 or Quark2 VPC accessory be used to just supply power, and use the coax connection for analog image?
Can the video format of Tau2, Quark2, and legacy Photon cameras be changed from NTSC to PAL (or PAL to NTSC)?
Do Boson, Tau2, or Quark2 meet any military environmental specifications or requirements?
Do Tau2 and Quark2 cameras support TTL-level communication?
Do Tau2 or Quark2 cameras allow for thermography and temperature characterization?
Does FLIR have any field failure rate data for Tau2, Quark2 that could be provided?
Does FLIR offer any kind of enclosure for Boson, Tau2 or Quark2 cameras?
Does FLIR offer discounts for educational institutions?
Does FLIR offer GSA pricing for Boson, Tau2, or Quark2 cameras?
Does FLIR offer or recommend software to run the gimbals, and what protocol does it use?
Does FLIR's SDK include support for Red Hat - Linux?
Does Muon have defective pixel replacement?
Does operating Tau2, or Quark2, or legacy Photon cameras at less than 9 Hz reduce the camera power consumption?